Part Number: DP83867IS
Other Parts Discussed in Thread: HD3SS3212
Hey Team,
I am planning on using the DP83867IS in a media conversion application where I am trying different transmission mediums. I would like to use the PHY in a back to back config where:
MDI <--> PHY <--> SGMII <--> Media <--> SGMII <--> PHY <--> MDI
I have two transmission mediums I will switch between using the HD3SS3212 passive switch. The first will be going to a fiber transceiver (SFP) that is on board so I have no concerns about drive strength here. The second media will be SMA coax of 50ohm impedance; full channel link looks like the following:
PHY <--> SGMII <--> HD3SS3212 <--> co-ax/fiber <--> HD3SS3212 <--> SGMII <--> PHY
My concern is based on the output drive of the 100Ohm diff. impedance SGMII signal and how long I can have the co-ax. I would like to attach a 1m cable but the following E2E post suggests that I will only get 18 inches total including board trace:
Is there a way to tell what the output current drive is and if I will need to add a line driver to the signal chain? Additionally, could you take a quick look at the switch to verify that it will work for this application? I see no issues with it when I read through the datasheet but having a second pair of eyes could help.
Bonus Question: Ideally instead of using SMA connectors I would like to use a Type-C cable for transmitting the 1GigE signal but USB is 90 Ohm diff. impedance. Do you have any tricks on an efficient way to run the signal over a Type-C cable? It would be very convenient so that I can run power to another board over the same cable as the test signals.
Best Regards,
Nick