Part Number: TUSB1310A
Is it possible to use only the USB3.0 part of the PHY and not connect any of the USB2.0 PHY signals.
From the datasheet I could determine what to do for most of the signals except a few.
Do I connect DM and DP to ground with a resistor if not used.
How do I connect VBUS if not used and will it influence the USB3.0 side.
Is the PHY_RESETn signal only for the USB2.0 PHY side or also for the USB3.0 side.
Anything else I should look out for if connecting only USB3.0 PHY.
Thanks
Manie