Part Number: USB-2-MDIO
Other Parts Discussed in Thread: DP83822EVM
Good afternoon,
I am trying to run USB-2-MDIO using the MSP-EXP430G2 Launchpad and the DP83822EVM board. I've made the connections from the Launchpad to the EVM as per the USB-2-MDIO User's Guide ( www.ti.com/.../snlu197.pdf ). On the EVM I have jumpers on J6 in the AVD INT position, the CT INT position, and the VDDIO INT position; the J2 jumper is in the 25MHz position; the J10 jumper is in the PU position; the J11 jumper is in the PU position. The MDIO pin of J14 of the EVM is connected to the P1.5 pin of the Launchpad. The MDC pin of J14 of the EVM is connected to the P1.4 pin of the Launchpad. GND of the EVM, GND of the Launchpad, and the GND1 turret of the EVM are connected to Ground of the power supply. The power supply is supplying 5V to the V+1 turret of the EVM. A Cat 5E cable is connected from J12 of the EVM to a link partner.
The AVD_LED of the EVM is lit. The VDDIO_LED of the EVM is lit. D4 (the link LED) of the EVM is lit.
The drivers are installed and the software successfully flashed onto the Launchpad. LED1 and LED2 of the Launchpad are fully illuminated and not blinking. The jumpers on J3 of the Launchpad are as per USB-2-MDIO User's Guide.
The Launchpad is connected to a computer via the USB cable that came with the Launchpad. LED0 of the Launchpad is lit. "MSP430 Application UART" shows up on the computer's device manager. USB-2-MDIO will open, and the baud rate and UART com port can be selected. Port can be opened, and Port Status reads "* HW Connected *"
However, when I run File > "Find PHY ID", all 32 PHY IDs show as "NOT available." Attempts to select a PHY ID and read registers or run scripts result in timeout errors.
I have tried using different cables connected to J12 of the EVM, and I have also tried leaving the other end of these cables disconnected from the link partner; still, all PHY IDs are not available.
Any idea what the problem might be?
Thank you!