Part Number: DP83822I
Hi
I have some question about EEE negotiation.
1) section 8.3.1.2 EEE negotiation
The device can be negotiated automatically it oneself if the RD pin is set bye external resistor.(It no need to set by external MCU)
Is my understanding correct ?
2) Regarding INT/PWDN_N pin, it is mentioned on the datasheet as below,
"To enable IEEE Power Down via INT/PWDN_N pin, the pin will need to be driven LOW to ground."
it mean that we should set the INT/PWDN_N pin to low(=ground) if we want to power-down. Does "LOW" mean ground?
Regards,
Koji Hamamoto