This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: LED pin current

Part Number: DP83867IR

I have a question for DP83867 pin current.

 

How much is the maximum allowed current on LED pins?

 

V_OL/OH is defined with I_OL/OH = +-4mA condition on the datasheet(SNLS484E, Section 7.5, P14)

So should we think +-4mA is maximum?

 

On the other hand, there is a figure about example strap connection on Figure 25(SNLS484E, P49).

In mode 4 case of this example, 470ohm LED is connected to LED pins through a diode.

Assuming diode VDD=3.3V, Vf=0.5V and V_OL = 0.6V, pin current is around 4.7mA in this case.

It is over 4mA! Can LED pins allow over 4mA?

 

Regards,

Oba