Part Number: TPS65986EVM
Other Parts Discussed in Thread: HD3SS460, TEST2, TPS65982
HI,
I do some tests with my design board and TPS65986EVM+HD3SS460 extension Board. These test and result listed blow,
- Board 1 : TPS65986EVM + HD3SS460 extension Board
- Board 2 : similar the Board1 but the GPIO setting is different (for DFP)
- Board 3: similar the Board 1 t the GPIO setting is the same (for UFP)
- Using "TPS6598x Configuration Tool" to get firmware of TPS65986
- Application : DFP (source for DP alt mode) send DP video and UFP (sink for DP alt mode) receive DP video
- Firmware 1: TPS65986 default firmware (burn form TPS6598x configuration tool)
- Firmware 2: By slva844a.pdf to use TPS6598x configuration tool to set and get firmware.( for DFP) only GPIO setting is set by board 2 circuit.
- Firmware 3: By slva844a.pdf to use TPS6598x configuration tool to set and get firmware.( for UFP).
Test1: DP Alt. mode function is good. (PASS)
Board 2(Firmware 2) --> DP video --> Board 1(Firmware 1, default) .
Test2: DP Alt. mode function is NG. (Fault)
Board 2(Firmware 2) --> DP video --> Board 1(Firmware 3) .
Test3: DP Alt. mode function is good. (PASS)
Board 1(Firmware 1, default) --> DP video --> Board 3(Firmware 3) .
Test4: DP Alt. mode function is NG. (Fault)
Board 1(Firmware 1, default) --> DP video --> Board 3(Firmware 1, default) .
Test5: DP Alt. mode function is NG. (Fault)
Board 2(Firmware 2) --> DP video --> Board 3(Firmware 3) .
Test6: DP Alt. mode function is good. (PASS)
Board 2(Firmware 2) --> DP video --> Board 3(Firmware 1) .
Tes7: DP Alt. mode function is good. (PASS)
Others PC (with USB-C) --> DP video --> Board 3(Firmware 3) .
Tes8: DP Alt. mode function is good. (PASS)
Board 2(Firmware 2) --> DP video --> USB-C to DP dongle .
My question is which parameters should be changed when using TPS6598x configuration tool? What is the setting of default firmware of TPS65986 EVM? Or in my application what setting should be concerned?
In Test 7 and Test 8 , onlly one device isn't TI chip, it seems good. why?
It seems only one device using slv844a.pdf to set firmware , the other is default EVM firmware. it seems still good. why?