This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DS90UB964-Q1: DS90UB964 setting problem

Part Number: DS90UB964-Q1

Tool/software: Linux

Hi:

i am use  one camera + ti ds90ub913 + ds90ub964,i only use one port,use ipu =0,csi =1,vc_id  = 1,now have some problem,i use the test core(mxc_v4l2_tvin.c),The following is the video of the test。

Q1:Video colors are all green。

Q2:Obviously used port0, but there have been four pictures

Q3:When I move the camera, the screen conversion is very slow, 10 seconds after the change

  • Hello,
    We received your question and an Apps engineer will review before we can provide a response.
  • Hi Qiyang,
    could you please show your project message with me through my email address steven-shi@ti.com? such as processor interfaced with UB964? application?...
    for your questions, please check:
    Q1:Video colors are all green。
    A: it seems the processor can NOT recover the correct raw data from "camera + UB964". Please check the camera sensor output spec. and UB964's register 0x73~0x76?

    Q2:Obviously used port0, but there have been four pictures
    A: the issue could be from the processor output format setting (which is connected with UB964). For UB964, you can only forward RX0 input to the CSI port.

    Q3:When I move the camera, the screen conversion is very slow, 10 seconds after the change
    A: the video display source is from the processor, so please check the processor output setting. thanks.

    best regards,.
    Steven