Other Parts Discussed in Thread: TUSB1002
Hi,
We want to set SLP_S0 high all the time, it's OK?
If it's OK, the comsumption of TUSB544 when it's connected and disconnected?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ,
The TUSB544 works as follows: the Upstream equalization indicates the EQ that will be applied to the receivers on the Upstream channel, as well as the Downstream equalization, indicates the EQ that will be applied to the downstream receivers. Meanwhile, the pins CFG0 and CFG1 configure both DC gains, the upstream and downstream and you can see in table 8 of the datasheet how to configure the CFG pins to the desired DC gain. The device has to be configured in this way because as you can see all 4 differential pairs are bidirectional, so It is easy to configure the gain without worry about the channel direction. (you can follow this rule: configure the EQ for upstream and downstream as all the differential pairs were inputs, and do the same for the DC gain considering all the differential pairs as outputs. THis will bring the adequate configuration regardless the channel direction).
Regards,
Diego.