Part Number: DP83822I
Hello,
I am interested in PMD to RMII transmit and receive latency numbers (there is another thread on that subject, but the answer has been kept private).
So far I have been assuming DP83848 numbers given in teh product datasheet and SNLA076A document (timing T2.26.4 and T2.27.5)
Can I get an update on these numbers for the DP83822 ?
Also, the DP83822 features the "RMII Recovered Clock Async FIFO Bypass" bit in RCSR regsiter. How the setting impacts the receive latency (latency with bit set and clear) ?. According to the datasheet, the bit is set by default. This is is strange given that the clear state (0) is described as "normal operating" mode. Is this a mistake ? I am running in RMII slave mode, so I guess this bit shall be cleared. Correct ?
In the same register, bit "RGMII TX Synced" to optimize transmit latency. Is there a similar bit available in RMII mode as running the MAC and the PHY out of the same reference clock would maybe allow some latency optimisation.
Thanks, Best regards
Pascal