Part Number: TPS2543
Hello Expert.
I'm sorry for the inconvenience caused by continuous posting.
I have two questions about DCP-auto mode.
1.
In DCP-auto mode there are divider 1 and divider 2.
This mode seems to be switched by detecting the output current,
but how long is this detection required?
How many seconds will the detection current be detected?
2.
When the mode switching is detected, if the output is discharged,
it is described in the data sheet, but once the power switch (FET) is turned off,
the internal discharge FET is turned on and the current flows to the GND side Do you?
Or is it the sequence of turning on the power switch (FET) again after setting the mode?
I am not familiar with this product, and I am seeking support.
Best,Regars.
Nori