This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB914 ASK Issue



Dear all:

      We have a problem about DS90UB914 ACK issue: 

      1. Application: Sensor - DS90UB913 - DS90UB914 - CPU

      2. When CPU write reset from 914/913 to sensor , Sensor ACK transmit to 913, but 914 no ACK transmit  to CPU.  

      3. This issue only occurs in Sensor reset command. when sensor reset, CLK wiill pulled low 500ms.

      4.  We set 914 register(0X03) to enable AUTO ACK , but also not produce ACK, Why is the function invalid?