Part Number: SN65HVD231
We use the SN65HVD231 in T-BOX,now we find one question is SN65HVD231 lost frames During transmission,What aspects are caused will be cause it ?could you help it and give me some suggestion how to solve it,tks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD231
We use the SN65HVD231 in T-BOX,now we find one question is SN65HVD231 lost frames During transmission,What aspects are caused will be cause it ?could you help it and give me some suggestion how to solve it,tks!
Darren,
Typically, when frames are lost the causes are:
1. Noise entering the bus and corrupting the transmission signals.
2. Incorrect termination resulting in reflections and incorrect voltage levels of the transmission signals.
3. Too much capacitance on the bus, resulting in "roll-off" of the waveform and the receiver incorrectly interprets the signals.
Along with several other reasons.
The termination looks correct in using the SPLIT pin, so I don't think that's the issue here. There is quite a bit of capacitance on the bus with the 100pF capacitors and the ESD diode, but not enough to cause message interpretation issues from my experience.
What kind of supply is being used to power VCC?
If the customer can lower the amount of capacitance on the CANH and CANL lines and still sees an issue, that can be ruled out. Also, what else the CAN bus connected to?
To really solve this issue, waveforms would be extremely helpful, so if there is any possible way of getting oscilloscope image captures, please do.
Regards,