Part Number: SN65LVELT23
Hello,
The output pin is connected to GPIO of MCU and is interrupt source. The input pins are connected to external connector without any termination resistors, and external connector is opened.
I attached a picture, ch3/ch4 are input pins(+/-) and ch2 is output pin of SN65LVELT23.
As you see, unexpected signal is generated on output when inputs are opened and interrupt is generated continuously on MCU so that MCU looks like stalled.
I cannot find out why signal appears on output pin. Which point can I check?