Part Number: TPS2513
Hi,
I have a PCB design question regarding current negotiation in USB powered devices. I have an application which require me to supply at least 1A of USB current. My plan was to make this application compatible with most of today's USB smart chargers (from Apple and others). My understanding is that there exists several ways to negotiate current from such devices, some have different voltage levels on D+ and D-, while others just short together D+ and D- etc. I found the TPS2513 in your product portfolio which is intended for USB charging of different devices. This is IC automatically detects the USB data line configuration, which enables connected devices to charge with their maximum supported current. My question is, can this same IC be used the other way around to actually make a USB powered device compatible with *almost* all USB chargers? My plan was to just use the TPS2513 and hook up the IN line to the VBUS line.
Do you see any issues with this approach, or do you have any better suggestions on how to do this? I can see one problem scenario where there is a TPS2513 on the charger itself and a TPS2513 in my application, would that cause a conflict?
Best regards,
Erlend