Part Number: DS90UB933-Q1
Hi Team,
Can you help me with this question?
I see in the datasheet that there is a 28bit message structure which is different depending upon whether or not you’re in 12-bit HF, LF, or 10-bit mode. I’m trying to understand what would happen if the 934 is configured for 12-bit mode and the 933 is running in 10-bit mode (due to a local side reset event, since the default register condition for 933 appears to be 10-bit mode)
Thanks, Dan
[LE-unlock]