This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: The latest Snapshot 3.05 tool doesn't let you always update the display name of the project

Expert 1025 points
Part Number: TPS65982


Struggled with this for a while.

I use 'Save Project' using the latest 'TPS6598x Application Customization Tool'. In the dialog there is a 'Display as:' box. However, if I decide to change the name, it doesn't work. It keeps the old name the next time I load the project. I can't even use the 'Project->Import Settings from Project', when I do this I get the previous name. I can't find a way around this, I can't change the display name once it is set the first time.