Part Number: TPS65982
Hi Team,
I want to configure GPIO behavior: After GPIO1 receive high then output high on GPIO2?
I did not see this setting option on TPS6598x Application Customizer tool.
Could you please help?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
Thanks for your help.
There are another GPIO question, please help to confirm.
Our application is Type C sink device, support 9V/12V/15V/20V PD power sink.
We want GPIO active high when 20V input, active low when 15V/12V/9V/5V input. But we didn't find Sink PDO Negotiated event on Mapped Event item.
Please help to confirm if there are suitable Mapped Event option can achieve the requirement?
Thanks