Part Number: TFP401A
Other Parts Discussed in Thread: TFP501, TFP401
Hi,
with reference to the TFP401A and the ref schematic from TI ( http://www.ti.com/lit/an/slla134/slla134.pdf
- pin 67 in datasheet pinout is DVdd but in same datasheet ref sch (fig 21 page 19) shows it as CAP and NOT connected to 3V3. Which is correct?
- pin 99 in datasheet pinout is RSVD but same datasheet ref sch (fig 21 page 19) shows it as PVDD2 and connected directly to 3V3. Which is correct?
- page 21 of datasheet says to use 0.01 (10nF) for each pin on Avdd, Dvdd etc but schematic shows 100nF. Stability is clearly important and there is very limited board space so we cannot put both. Which is recommended?
Many thanks
Riccardo