Part Number: TPD4E1U06
Should the ground pin of protection diodes be connected to the chassis ground or the digital ground? Would you answer this question differently for Ethernet or USB?
I am using the TPD4E1U06 to protect my Ethernet and USB data lines.
My "chassis grounds" are the metal jacket surrounding an ethernet RJ45 jack and USB jack. The reference design for TI's DK-TM4C129X dev kit separates the metal jacket of an Ethernet plug to digital ground through a 1MOhm and high voltage cap (page 30): http://www.ti.com/lit/ug/spmu360a/spmu360a.pdf
The diodes (D14) used for Ethernet are only differential; I'm not following the example directly. I have the same question for the USB connection on the same page. The example shows the ESD diodes D5, D6, and D7 going strait to digital ground. Wouldn't you be more protected if those diodes went through R36? Why treat zaps on the connector shield different from zaps on the data bus?