This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2553: TPS2553

Part Number: TPS2553


Dear Guys,

Pls help for issue when we test TPS2553 EVM.

I’m trying to test the reverse-voltage protection of TPS2553, as shown in the following figure.

 

Here’s my test setup.

  1. Turn on CH1 (5.0V) on DC power supply.
  2. Connect a 5-ohm resistor or an E-load with 1A constant-current load at Vout of TPS2553 EVM.
  3. Turn on CH2 (5.5V) on DC power supply.
  4. Observe the FAULT pin on TPS2553EVM.

 

However, I have difficulty having FAULT pulled low (active) when a reverse voltage (5.5V) is applied to Vout.

Could you help me understand what might be wrong?

Thanks, Ian.