Part Number: TPS2553
Dear Guys,
Pls help for issue when we test TPS2553 EVM.
I’m trying to test the reverse-voltage protection of TPS2553, as shown in the following figure.
Here’s my test setup.
- Turn on CH1 (5.0V) on DC power supply.
- Connect a 5-ohm resistor or an E-load with 1A constant-current load at Vout of TPS2553 EVM.
- Turn on CH2 (5.5V) on DC power supply.
- Observe the FAULT pin on TPS2553EVM.
However, I have difficulty having FAULT pulled low (active) when a reverse voltage (5.5V) is applied to Vout.
Could you help me understand what might be wrong?
Thanks, Ian.