Part Number: DS100MB203
Hi,
I hope this is not a stupid question.
Do I need to consider the polarity of my inputs signals on the DS100MB203?
So, can I connect the P(ositiv) end of my DUT to the IN- input and except it will appear on the OUT- output?
This figure seems to show it is not possible:
If not possible, is there another way if I dont want to rely on the polarity inversion feature of the PCI express bus?
Thanks and BR
Elias