This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROTECTION

Guru 13485 points

Other Parts Discussed in Thread: TVS3300

I am looking for TVS Bi-directional (back-to-back TVS Zener)

 Standoff Voltage 36v

Case 0603 or 0805

ESD protection ±30kV contact discharge

Quality: better AEC-Q

  • Hi Eli,

    We currently do not have a device that matches your requirements above. The closest device that matches your description is the TVS3300, a single channel unidirectional surge protection device that offers 35A of surge protection and 14kV contact/30kV air gap ESD protection.