Part Number: TUSB522P
Other Parts Discussed in Thread: SN65LVPE512, TUSB522P, TUSB8044
Hi,
If we have applications that may place two USB3.0 gen1 (5Gbit/sec) redtriver parts in series, because of high loss, will this work? We have both the TUSB522 parts as well as the SN65LVPE512 parts in designs. Will the USB3.0 jitter requirements still be met? Would there be other SI effects to worry about? We would need to consider cases with two TUSB522 parts in series, a TUSB522 in series with a SN65LVPE512, and two SN65LVPE512 parts in series. Realize that the SN65 part is not recommended, however, we have some systems built with this part.
In situations with high USB line losses, is it a good idea to place a hub part downstream from the host in an effort to "retime" the USB channel, possibly also putting redriver parts on both sides of the hub?
Thank you,
Bruce