We need a usb hub to work with a usb wifi and 3 usb cameras. We want to on/off cameras and wifi with a control card. Our supplier designed a usb hub for us. But we cant get camera images with this hub.
The hub works with a mouse. Also it shows cameras but there is no image (black screen) and the resolution is only 160x120. We can not increase the resolution also. We think that the usb hub works at low speed mode. Becasue when a usb flash disk is connected the write/read speed is 1 Mbit/sec.