Part Number: MAX3223
Hi I am using MAX3223 device in my design. And I have 2 PHYTEC processors in my overall system [ 2 mother boards].
I need to have 2 separate UART/RS232 connectors for getting system logs, one per PHYTEC.
So i need to have UART to RS232 line drivers in my design.
Since MAX3223 is a dual channel line driver can i connect 2 separate UART ports to MAX3223 device and take 2 separate RS232 signals and provide to RS232 connector?
With the RTS and CTS in picture (with flow control in picture) only one fully functional UART/RS232 translation can be achieved with MAX3223 device and since I am not using RTS and CTS, I am thinking to use 2 separate UARTS with MAX3223 chip. Need advise on this.