This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS91M040: DS91M040 current consumption

Part Number: DS91M040

Hi everybody!
About TI's DS91M040 125 MHz Quad M-LVDS Transceiver
I 'd like to request for more described information.
Applicable IC data sheet: SNLS 283 M,
[DC Electrical Characteristics / SUPPLY CURRENT]
Driver Supply Current 67 mA - Typ 75 mA - Max
Receiver Supply Current 32 mA - Typ 38 mA - Max
Does this current consumption include the operating current of all 4 ch transceivers?
If you include the operating current of all the transceivers, when you stop individual elements
What is the current consumption? In case of
(For example, when using only one driver enable and other Disable, is it possible to think that it is 1/4 current consumption?)
Best Regards
Shing