Part Number: TUSB546EVM
I want to know the function for CONFIG1 and CONFIG2 of DP interface.
and I want to know if the two pin wires connecting to DP host could be removed in TUSB546EVM.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB546EVM
I want to know the function for CONFIG1 and CONFIG2 of DP interface.
and I want to know if the two pin wires connecting to DP host could be removed in TUSB546EVM.
Thanks
Hi Hardy,
These pins are used in DP dual mode when the source is transmitting HDMI video AC coupled, then you need a level shifter to have HDMI DC coupled signals.
CONFIG1 -> Cable Adaptor Detect (CAD), this is high when a level shifter is connected to send HDMI video.
CONFIG2 -> Consumer Electronics Control (CEC) this is an HDMI signal, it is used to control your media devices connected through HDMI using just one remote control.
if they are not used, you still need the 1M pull-down on CONFIG1 and 5M pull-down on CONFIG2.
Regards
Hi
thanks for your reply.
this is only for DP application.
local has checked the DP Standard V1.4 chapter 3.2.1 about CONFIG1&CONFIG2 descriptions,
There is a bit different from your feedback, both the two pin should be pull-down with 1Mohm.
and pls help check if the DP host side has the pulldown resistor, should we remove the pull-down resistor from the DP physical interface side? thanks.
DP host side in PC main board ----> DP physical interface
Hi Hardy,
For DP only, the resistors can be 1M ohms or larger.
The resistors are commonly placed close to the connector, it shouldn't be a problem if the resistor is close to the host.
Regards
Hi
thanks for your reply, another quesiton is that, if i can remove the two pin connnection between the connector and DP host if it is only for DP application, so that i can use less wilres to connect the connector and DP host which can be cost down for the system design.
thanks.