Part Number: SN75DPHY440SS
Hi ,
I'm searching a method to extend MIPI CSI-2. In our application , Camera and Application processor is splitted on two side. The distance between them is 1 meter. Can sn75dphy440ss be uesd? If one sn75dphy440ss uesd in Application processor side can't work , Can we use two sn75dphy440ss, one in camera side for Pre-emphasis, the other one used in Application processor side for equalization ?