Part Number: DS280DF810
Hi
I find the description of DS280DF810 as "Including Sub-Rates Like 10.3125 Gbps, 12.5 Gbps, and More".
Does it also can support 16GFC (14.025G)? If yes, which register or setting I should modify?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS280DF810
Hi
I find the description of DS280DF810 as "Including Sub-Rates Like 10.3125 Gbps, 12.5 Gbps, and More".
Does it also can support 16GFC (14.025G)? If yes, which register or setting I should modify?
Thanks
Hi,
The DS280DF810 retimer part number does indeed support 14.025Gbps rate in retimed mode. The user can program the retimer channel(s) in question to this rate via the SMBus channel registers settings below:
Addr Value Comment
0x60 0x20 14.025G rate (28.05G)
0x61 0x46 14.025G rate (28.05G)
0x62 0x20 14.025G rate (28.05G)
0x63 0x46 14.025G rate (28.05G)
0x64 0xFF Max PPM tolerance
0x18 0x10 Set to divide by 2
0x09 0x04 Enable divider select override
Cordially,
Rodrigo Natal
HSSC Applications Engineer