Part Number: DP83867E
Hi
I have questions of DP83867E.
1. Power supply
We can see the description of POWER pins like "Each pin requires a 1uF and 0.1uF capacitor to GND" in Pin Functions of Datasheet.
If these capacitor is not offered at each supply pins, what impact can be considered?
For example, the following capacitors and connection can be acceptable?
2. JTAG port
We would leave JTAG port open because it is not in use.
What is the purpose of JTAG port?
Can user access the register of DP83867E by JTAG interface?
3. EVM setting
In DP83867E EVM, RX_CTRL doesn't have external strap resistor (open) and it means RX_CTRL is MODE 1 according to datasheet.
However, RX_CTRL of MODE 1 is not available. How does EVM work in this case?
BestRegards
BestRegards