Part Number: DS90UB929-Q1
Hello,
We are using the DS90UB929-Q1 devices. There are times when the device is powered on and it appears to be partially locked up. We have a EEPROM for EDID info to an HDMI I2C shared channel with the serializer. When the serializer appears to be locked up it holds the DDC-I2C bus high disabling the HDMI interface access to the EEPROM. If we let the device sit unpowered for a period of time, it all of the sudden works fine. I went back and verified all power rails appear to be stable and the PDB line is isolated and timed properly. RES0,1 to GND. RES2 thru 50ohm to GND. NC0-8 are truely No Connects. Thoughts ?