This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1219: the power supply of LMH1219

Part Number: LMH1219


Hi Team,

Could you please tell us how to set  the VDD_LDO? 1.8V or 2.5V?

Best Regards,

jianguo

  • Hi Jianguo,

    VDD_LDO is always 1.8V. Setting VDD_LDO depends on whether you operate in Single Supply 2.5V mode or Dual Supply 2.5V/1.8V Mode.

    • Single Supply 2.5V Mode: Provide 2.5V to VIN. When this is done, VDD_LDO is an output, so you will only need an external 1uF and 0.1uF bypass capacitor to VSS. Do NOT provide 1.8V to VDD_LDO, since VDD_LDO is an LDO output in this mode.
    • Dual Supply 2.5V/1.8V Mode: Provide 1.8V to VIN and VDD_LDO. Meanwhile, provide 2.5V to VDD_CDR and VDDIO.

    For more information. refer to Section 9 of the datasheet (Power Supply Recommendations).

    Thanks,

    Michael

  • Hi Michael,

    Thank you for your support.
    I understood it.

    Best Regards,
    Jianguo