This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A-Q1: Can DS90UB913A support 1920 * 1080 30fps camera module?

Genius 4905 points

Part Number: DS90UB913A-Q1
Other Parts Discussed in Thread: DS90UB933-Q1

Hi, E2E members

I would like to check to you if DS90UB913A can support 1920 * 1080 30fps camera module.

Camera module setting is here.
- Bus Width: 8-Bit (YUV)
- Active Picture: 1920x1080
- Total Frame: 2200x1125
- Pixel Clock: 2200*1125*30FPS=74250000Hz=74.25MHz

As you know, DS90UB913A can support 10-bit Payload up to 100 MHz and connect a 8-bit data camera module.

From the data sheet and following E2E.
e2e.ti.com/.../428578

I think DS90UB913 should be ok, but may you please help double check?

Regards,
Nao