Part Number: TMDS181
Hi dear supporting team,
my customer is evaluating XILINX evk with TMDS181 on it, the setup is camera input to TMDS181, and then to FPGA. the sch is as attached.
while they found there is no output even there is singal input to our chip. and they are running at HDMI2.0, TMDS181 powering up with default setting.
pls help comment which regs need be changed. tks!
regisiter address offset(hex) | value(hex)
0x0 0x54
0x1 0x4D
0x2 0x44
0x3 0x53
0x4 0x31
0x5 0x38
0x6 0x31
0x7 0x20
0x8 0x1
0x9 0x2
0xA 0xB1
0xB 0x0
0xC 0x0
0xD 0x0
0xE 0x0
0xF 0xF
0x10 0x0
0x11 0x0
0x12 0x0
0x13 0x0
0x14 0x0
0x15 0x0
0x16 0x0
0x17 0xF0
0x18 0x0
0x19 0x0
0x1A 0x0
0x1B 0x0
0x1C 0x0
0x1D 0x0
0x1E 0x0
0x1F 0x0
0x20 0x4A