Part Number: TMDS181
Other Parts Discussed in Thread: TMDS171
Hi,
My customer have been looking at the TMDS181 redriver/timer IC but have some questions in that regard. Could you please look into this?
- When running device in I2C mode the TX_TERM_CTL setting is fully defined by software. Is there a way to automatically switch termination in this case? Setting “01” is listed as reserved. I2C gives highest flexibility w.r.t. setup however HW mode has automatic termination when TX_TERM_CTL = NC.
- Register 0x0A has bit 7 defining “Application mode selector” between 0: Source and 1: Sink (default). What does this change in the device configuration?
- The “EyeScan” Tool has options to set DDC slew rate – however the registers are not specified in the datasheet?
- We might be going for DDC snooping. However this puts extra capacitive load on the lines. How much is the capacitive load on the SDA_SRC/SCL_SRC and SDA_SNK/SCL_SNK pins?
Thanks. B.r /M.A.M