Part Number: TCA6424A
Hello,
I using a TCA6424A to read inputs and I have some questions:
1) In the datasheet, I did not find after doing a RESET pulse, what will happens with the INT pin, if INT is asserted and the device is reseted, will the INT be cleared?
2) In the datasheet says "Resetting the interrupt circuit is achieved when data on the port is changed to the original setting or when data is read from the port that generated the interrupt"
About this original setting, how long takes it to consider an original setting? If I switched the input high -> low , low -> high, is there any time to respect this "original setting", or the device will consider the last read as original setting and no matter how much time occurs the change, if turned it back, the INT will be cleared?
3) In this topic e2e.ti.com/.../518072 saying that unconnected pins should be left unconnected, but for "extra caution" you can PU then externally. Where in the datasheet says about this internal pull up? How strong is this pull-ups? Are they referred to Vccp?