This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS181: About TX_TERM_CTL=NC(Automatically selects the termination impedance)

Guru 21045 points

Part Number: TMDS181

Hi Team,

 

Our customer would like to about TX_TERM_CTL=NC(Automatically selects the termination impedance).

They are evaluating a signal of 4k60(6Gbps) from VGA.

Therefore, we believe that setting of “TX_TERM_CTL=NC” is most suitable.

 

Could you please let us know if you have any concern?

(For example, this setting cannot pass a compliance test etc.)

 

Regards,

Kanemaru

  • Hi Kanemaru,

    The best option is TX_TERM_CTL=NC, in this test the Tx termination will be selected from the data rate and HDMI version.

    For HDMI1.4 there are two options:

    Data rate < 2Gbps -> No termination

    Data rate > 2Gbps(< 3.4Gbps) -> 150 to 300 ohms differential termination

    For HDMI2.0 there is just one option

    Data rate > 3.4Gbps -> 75 to 150 ohms differential termination

    Regards

  • Hi Moises-san,

    Thank you always for your kind support and information.

    Regareds,

    Kanemaru