Part Number: UCC21225A
Other Parts Discussed in Thread: UCC27211
Hello.
I am evaluating UCC21225 and I have a question.
Please check the attached document
thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Masazumi-san,
On the above experiment, you mentioned removing CBOOT, and applying the voltage to VDD and still observe that the SW node can still rise. There is still a path from HB to the SW node with the floating high side driver.
Can you try the same with removing the boot diode? In this case there should not be any path for the current to flow from VDD to the SW node.
In your design, is there expected to be a high resistance, or impedance on the SW node? This is not usually the case.
One difference I see in the UCC27211, and the UCC21225 is the UCC27211 has lower HB quiescent current of 0.1mA Vs 1.0mA for the UCC21225.
Regards,
Richard Herring