Other Parts Discussed in Thread: TL16C554A, TL16C554
High,
are there any app notes how to migrate from 16c554 to 16c554A?
As far as I understand is the is the A-revision capable of operating at both 5V and 3,3V. According to the datasheet the electrical parameters at 5V operation are almost the same as the 16c554.
Th only significant difference I found are the AFE Functions ( Bit 5 of MCR). So if my Sw leaves the AFE bit unchanged the 16c554A should be fully compatible with the 16c554 (without index).
Is this correct or are there any other traps?