This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: SN65DSI86 eDP source PHY test

Part Number: SN65DSI86

Dear all,

My customer want to do the eDP Source PHY Compliance test to verify if SN65DSI86 can meet the requirement, according to the test method, eDP source need be set in certain ways, so they need us provide the tool/script to get the pattern, rate, swing and pre-emphasis setting, can we provide the relevant materials for the test?

 

Thanks.

  • Hello John,

    We can provide a customized script based on the selected panel spec. You will need to provide the panel's EDID.

    You can use the attached script as a reference.

    <aardvark>
        <configure i2c="1" spi="1" gpio="0" tpower="1" pullups="0"/>
        <i2c_bitrate khz="100"/>
    
    ======Page 7======
       <i2c_write addr="0x2D" count="1" radix="16">FF 07</i2c_write> />
    
    ======ASSR Control to RW from R-only.  TEST2 pin must be high at rising edge of EN pin ======
       <i2c_write addr="0x2D" count="1" radix="16">16 01</i2c_write> />
    
    ======Page 0======
      <i2c_write addr="0x2D" count="1" radix="16">FF 00</i2c_write> />
    
    ======Disable HPD======
      <i2c_write addr="0x2D" count="1" radix="16">5C 01</i2c_write> />
    
    
    ======Single 4 DSI lanes======
    
      <i2c_write addr="0x2D" count="1" radix="16">10 26 </i2c_write> <sleep ms="10"/>
    
    ======DSI CLK FREQ======
      <i2c_write addr="0x2D" count="0" radix="16">12 </i2c_write> <sleep ms="10"/>
       <i2c_read addr="0x2D" count="2" radix="16">00</i2c_read> <sleep ms="10"/>
    
    
    ======enhanced framing======
    
      <i2c_write addr="0x2D" count="1" radix="16">5A 04 </i2c_write> <sleep ms="10"/>
    
    
    ======ADDR 0x93 CFR======
    
       <i2c_write addr="0x2D" count="0" radix="16">93</i2c_write> <sleep ms="10"/>
    
    ======Read======
        <i2c_read addr="0x2D" count="6" radix="16">00</i2c_read> <sleep ms="10"/>
    
    ======Pre0dB 2 lanes no SSC======
       <i2c_write addr="0x2D" count="1" radix="16">93 30</i2c_write> <sleep ms="10"/>
    
    ======L0mV HBR======
       <i2c_write addr="0x2D" count="1" radix="16">94 80</i2c_write> <sleep ms="10"/>
    
    ======PLL ENABLE======
       <i2c_write addr="0x2D" count="1" radix="16">0D 01</i2c_write> <sleep ms="10"/>
    
      <i2c_write addr="0x2D" count="0" radix="16">0A</i2c_write> <sleep ms="10"/>
    
       <i2c_read addr="0x2D" count="2" radix="16">00</i2c_read> <sleep ms="10"/>
    
    ======PLL ENABLE======
       <i2c_write addr="0x2D" count="1" radix="16">0D 01</i2c_write> <sleep ms="10"/>
    
      <i2c_write addr="0x2D" count="0" radix="16">0A</i2c_write> <sleep ms="10"/>
    
       <i2c_read addr="0x2D" count="2" radix="16">00</i2c_read> <sleep ms="10"/>
    
    ======POST2 0dB ======
       <i2c_write addr="0x2D" count="1" radix="16">95 00</i2c_write> <sleep ms="10"/>
    
    
    
    ======Semi-Auto TRAIN ======
       <i2c_write addr="0x2D" count="1" radix="16">96 0A</i2c_write> <sleep ms="20"/>
    
    
    ======ADDR 0x0A CFR======
    
       <i2c_write addr="0x2D" count="0" radix="16">96</i2c_write> <sleep ms="20"/>
    
    ======Read======
        <i2c_read addr="0x2D" count="1" radix="16">00</i2c_read> <sleep ms="10"/>
    
    =====CHA_ACTIVE_LINE_LENGTH=======
        <i2c_write addr="0x2D" count="2" radix="16">20 80 07</i2c_write> <sleep ms="10"/>
    
    =====CHA_VERTICAL_DISPLAY_SIZE=======
        <i2c_write addr="0x2D" count="2" radix="16">24 38 04</i2c_write> <sleep ms="10"/>
    
    =====CHA_SYNC_DELAY=======
        <i2c_write addr="0x2D" count="2" radix="16">28 00 00</i2c_write> <sleep ms="10"/>
    
    =====CHA_HSYNC_PULSE_WIDTH=======
        <i2c_write addr="0x2D" count="2" radix="16">2C 20 80</i2c_write> <sleep ms="10"/>
    
    =====CHA_VSYNC_PULSE_WIDTH=======
        <i2c_write addr="0x2D" count="2" radix="16">30 05 80</i2c_write> <sleep ms="10"/>
    
    =====CHA_HORIZONTAL_BACK_PORCH=======
        <i2c_write addr="0x2D" count="1" radix="16">34 42 </i2c_write> <sleep ms="10"/>
    
    =====CHA_VERTICAL_BACK_PORCH=======
        <i2c_write addr="0x2D" count="1" radix="16">36 17</i2c_write> <sleep ms="10"/>
    
    =====CHA_HORIZONTAL_FRONT_PORCH=======
        <i2c_write addr="0x2D" count="1" radix="16">38 30</i2c_write> <sleep ms="10"/>
    
    =====CHA_VERTICAL_FRONT_PORCH=======
        <i2c_write addr="0x2D" count="1" radix="16">3A 03</i2c_write> <sleep ms="10"/>
    
    =====DP_18BPP_EN =======
      <i2c_write addr="0x2D" count="1" radix="16">5B 01 </i2c_write> <sleep ms="100"/>
    
    =====COLOR BAR =======
        <i2c_write addr="0x2D" count="1" radix="16">3C 10</i2c_write> <sleep ms="100"/>
    
    ======enhanced framing and Vstream enable======
    
      <i2c_write addr="0x2D" count="1" radix="16">5A 0C </i2c_write> <sleep ms="100"/>
    
    ======DUMP CFR======
        <i2c_write addr="0x2D" count="0" radix="16">20</i2c_write> <sleep ms="10"/>
    
    ======Read======
        <i2c_read addr="0x2D" count="32" radix="16">00</i2c_read> <sleep ms="10"/>
    
    
    
    </aardvark>
    

  • Thanks Joe, any help I will contact you.