Part Number: DP83816
Other Parts Discussed in Thread: DP83847,
Hello,
I checked the register of the DP83847 and application note.
I understood how to configure for the compliance testing roughly.
-----------------------------------------------------------------------------------
// software reset (clear register)
// program DUT to 100Base-TX mode
// program DUT to Pseudo Random bit sequence output
// digital reset (doesn't clear register)
----------------------------------------------------------------------------------
I checked the register of the DP83816, have some questions.
address 0000h bit 8 : Reset
address 0080h bit 15:Reset
Q1) Which should I use above two address for software reset?
address 0080h bit 13 : 100Mb/s
address 0080h bit 8 : Full duplex operate
address 00E4h bit 11 : PSR15
address 00E4h bit 9 : BIST start
Q2) Does it need digital reset? If the answer 'yes', which address should I configure?
Q3) Although the DP83816 have PCI Media Access Control,
does it need to program DUT to Forced MDI or MDIX mode?
Best Regards,
Naoki Aoyama