Part Number: DS90UB964-Q1
Hi Tier,
I have two question for this chip debug:
1 the Round Robin mode is used and format register's 0x71 bit 7/6 are set 00. RX0 and RX1 use same virtual channel id. we can get camera data and preview picture; But in this mode, according datasheet's decription, its request is different virtual id. We get blink picture. two camera pictures are overlapping. Could you please explain this situation?
2 in the Line-Concatenated Forwarding mode, Rx0 and Rx1 can use same virtual channel id, the senor data format register value is 0x2c, and enable line-concatenated forwarding mode by the register 0x21.
I'm sure that sensor data format regiser 0x71 and CSI0_SYNC_FWD 0x21 are written rightly. in this situation, our SOC MIPI combo can't get right sensor data format 0x2c. it can't process data, so we can't preview camera data. Could you please expain this?