Part Number: TPS25740
Hi Team,
Could TPS25740 support up to 100W, 20V /5A output ?
And is there any Automotive Q1 grade plan for this part ?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25740
Hi Team,
Could TPS25740 support up to 100W, 20V /5A output ?
And is there any Automotive Q1 grade plan for this part ?
Thanks.
HI Rocson,
Yes the TPS25740 is capable of 100W 20V/5A output. The TPS25740's voltage advertisment are as follows: 5V,12V,and 20V all at either 3A or 5A.
If you are interested in a superset of this, please take a look at the TPS25740B as it does the same the TPS25740 but it also includes the 15 voltage advertisment option.
As it is, there are no plans to have an automotive qualified (Q1) version of the part.
Regards,
Jimmy Hua
Hi Donovan,
Thanks for your explanation.
So for TPS25740, it should also work to output 100W, when one 5A qualified cable with E-mark is used ? Or as you mentioned before, TPS25740 would not talk to cable, so when one 5A cable with E-mark is attached, it would not output 100W ?
Also, Do you know the TPS25740B -Q1 automotive version device RTM schedule ?
Thanks for your help.