Part Number: PCA9557
hi dear supporting team,
what's the max junction temp of PCA9557PWR? there is no information in d/s. and from calculation, the max power consumption at 3.6V is only 0.079mW, is this correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Vera,
Unfortunately, we do not specify the max operating junction temperature. Instead we specify the Max Operating free-air temperature which uses the JEDEC standard for the PCB. Max power consumption depends on a lot of variables. First, how many of the devices will be inputs and how many will be outputs? The outputs can drive up to 24mA depending on Vol. Generally speaking the IO don't drive large loads, so the power dissipation doesn't normally high. But if driving higher loads then you need to figure out the max power dissipations (Pdis) because it can add a large delta for air to junction temperature.
Where did you get the 0.079mW? That comes out to 21.9 uA. You could have much higher loads than that depending on how the part is used.
If the power dissipation is low then the temperature differential between the ambient air (Ta) and the junction temperature (Tj) will be small and you can approximate the max junction temperature to be the max operating free air temperature. We guarantee our specifications based on max free-air temperature based on JEDEC standard. I wished we do it this way but it has been done this way for a long time on these types of parts. My opinion is that we should spec and test our parts based on max junction temperature because the thermal resistance from Air to Junction varies to much, which the thermal resistance from junction to case does not, and you can measure the case temperature with a thermal couple which is very accurate.
Let me know if this is clear and if there is anything else you need clarification on.
-Francis Houde
hi Francsis,
thanks for the reply!
yes, I got the 0.079W from the Iq, so for I load of 24mA, could I calculate the power consumption in this way: 0.079W+3.6*24mA?
actually I don't have specified operating condition, this is request by customer's sourcing team, they just want to do investigation on the chip. tks!