This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: output 50 ohm impedence

Part Number: DP83867IS

Hi,

We are intending to use the DP83867ISRGZ in tow of our new designs. According to the datasheet pg. 86, the device has controlled impedance for MAC I/Os. Despite using the term “I/O” I believe this is only available for the MAC outputs:

 

TX_CTRL

GTX_CLK

TX_D[0:3]

 

Can you verify if only these signals I have listed include the output 50 ohm impedance?

Thanks,

David