Part Number: DP83822IF
Hi Guys,
I'm hoping to use the DP83822IF to interface between my RJ45 twisted pair Ethernet bus and the Zynq7020 RGMII MAC layer. I've just noticed that the MDIO bus (MDIO, MDC) is part of the RGMII protocol and is used for device config and monitoring. I'm wondering will the DP83822IF work OK without the MDIO at it's default settings? Is it capable of detecting speed etc without this interfacing?
Your help would be much appreciated.
Many Thanks,
Dave