Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2544: TSP2544 Version for using with 9V and 12V Supply

Part Number: TPS2544

Hello All,

I am using TPS2544 for my application, which is to charge mobile devices in DCP mode from any USB power source.As the maximum voltage that can be applied to IC is 7v, our application needs an IC with similar features and characteristics but with higher voltage rating.

Is there any version of the IC whose rating can go upto 9v and 12 v  for charging in DCP modes?Please help!

Thanks,

Chaithanya.S