Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB928Q-Q1: PDB and LOCK time

Part Number: DS90UB928Q-Q1

Hi team,

From the datasheet, we can see lock timeTddlt=6-40ms, Vih(min)=2.0V, Voh(min)=2.95V.

However, in my customer's board, we got below test result, Lock pin ramp up earlier than PDB voltage. Could you kindly explain this?  See schematics below, Lock is connected to MCU I/O pin without pull-up or pull-down resistor.

Dongbao