Part Number: DS90CF384A
Hello, I am using DS90CF384AMTD to interconnect LVDS from the controller to a RGB LCD. Have used RxOUT0-27 as RGB+Control signals as shown in the pg#5 of the datasheet (Figure 4. “16 Grayscale” Test Pattern (DS90CF384A)). But we don't see any image in the LCD. I measured proper 50MHz clock art RcCLK, but the RES pin is keep on toggling and all the R,G,B signals also look noisy. (*Note*: LCD controller SW is also not complete, It is configured for a LVDS LCD with different resolution, so it can be a SW issue as well). What are the basic checks I can do to ensure that there's no hardware issue. Please find attached my schematics and suggest. Thanks.